Loading
Blog | Cybersecurity
Recent ActivityRecent Activity
3 minute read

IoT Security: Hardware Root of Trust

What is Hardware Root of Trust and Why is it Important for Digital Security?

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Engineer working in factory holding and iPad

IoT has steadily gained popularity in recent years with more users migrating to digitalized products and smart gadgets. As an increasing amount of IoT equipment comes online, many unsecured items will be vulnerable to remote software assaults. Inadequate security gives hackers the opportunity to brick and commandeer a device to help build botnets. These malware networks introduce unauthorized code, steal data, or exploit their hosts through some other means. Because device manufacturers want to safeguard their reputations, their IoT devices must be secure

. With more laws, regulations, and standards being created in this vein, security cannot be imposed as an afterthought. This is where Hardware Root of Trust comes into play.

What is Hardware Root of Trust?

Root of trust establishes the secure process boot up chain, called Chain of Trust, used to validate software and hardware used on the device. If the credentials used to implement the initial piece of code are verified, each successive piece of code executed is trusted. A strong root of trust consists of identity and cryptographic keys rooted in the hardware of a device. This establishes a unique, immutable, and unclonable identity to authorize a device in a network. It enables a secure boot process using keys for cryptographic operations, ensuring the authenticity of firmware and software until the OS (Operating System) is loaded.

How is Hardware Root of Trust Implemented?

Hardware root of trust can help with a range of security issues that are primarily divided into pre-boot and post-boot. Pre-boot can use a computer chip called a Trusted Platform Module (TPM) to verify/measure integrity and secure the boot process from low-level malware. TPM assists with various activities during post-boot, including root of trust for authentication. Systems that deploy hardware root of trust will use unified extensible firmware interface (UEFI), which offers options such as “Secure Boot” that help prevent attacks or infection from malware.

How does the Root of Trust process start inside a processor?

There are essentially two methods: the battery backed storage of secret keys and Physical Unclonable function (PUF). PUF is widely held as the industry standard for FPGAs and ASIC processors. PUF starts with a physical microstructure. These microstructures can be random imprints of some substance, such as foam, plastic, or even silicon. The processor then uses challenge response authentication to measure this random structure. (Most people know challenge response authentication as username/password - ask for a username, type a username.) These random measurements work in the same way: the processor measures something withing the microstructure, and the microstructure is measured and validated. The problem with cloning, or making the process unclonable, is ensuring the manufacturing process could not replicate the microstructure.

What are some of the other phases of Hardware Root of Trust?

Typically, solutions start with an Immutable Boot Loader (sometimes using a PUF), which then starts the BIOS (Basic input/output System) or UEFI validation process. The Phase 1 process uses RSA or ECC private key encryption, sometimes using a TPM to build the keys necessary for the RSA and ECC cipher suites. If an OS is used, the loader is validated using the same private key encryption, then finally the OS, and application (if used).

What other hardware might be necessary for Hardware root of Trust?

If startup speed is a factor in your design, SSL accelerators can offload some of the algorithmic horsepower typically done by the main processor. There are now chipsets built for this specific purpose. Entropy generating hardware can be used to achieve proper random Key generation, although a PUF can also be used, to some degree.

If you would like to delve a little deeper into hardware root of trust, check out our TechTalk

. To learn more on how to get easy industrial device communication that is reliable and secure visit our embedded index page: Anybus Embedded Index
.

Published September 21, 2022

Industrial Cybersecurity Solutions
Industrial zone,The equipment of oil refining,Close-up of industrial pipelines of an oil-refinery plant,Detail of oil pipeline with valves in large oil refinery.
Industrial Cybersecurity Solutions

Reliable OT Cybersecurity solutions from the leader in industrial automation. Learn more about our technology & solutions.

Learn More
Topics: Hardware

Rob Lodesky
Rob Lodesky
Key Account Manager, HMS Networks
Rob is on his 9th year at HMS Industrial Networks and currently holds the role as a Key Account Manager. Rob has worked in various roles within the Automation and industrial communication industry since 2005.
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right