Loading
Case Study | PlantPAx
Recent ActivityRecent Activity
4 minute read

Next generation technologies support mining productivity and innovation capabilities

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Next generation technologies support mining productivity and innovation capabilities hero image

Challenge

  • Provide services to support project design, build and commission the new Amrun bauxite mine and associated processing and shipping infrastructure.

Solutions

  • Rockwell Automation Global Solutions provided engineering design, equipment supply and implementation services.
  • An integrated process control system with PlantPAx® delivering plant-wide control and Allen‑Bradley® GuardLogix® and CompactLogix™ delivering integrated control across the site.
  • Safety at the forefront with functional safety management plans, risk assessments and GuardLogix controllers integrated with the PLCs to provide seamless visibility of safety and control.
  • Next generation information solutions with FactoryTalk’s® suite of products delivering insights and visibility into the system with local and remote access, and mobility tablets enabled by ThinManager® provided access to real time information.

Results

  • Contributed to smooth commissioning through PlantPAx library delivering significant cost and scheduling savings and detailed Factory Acceptance Testing simulating control of plant from the dump truck to the ship loader.
Main Image

Rio Tinto’s Amrun bauxite mine is located in Far North Queensland on Cape York in Australia. Photo courtesy of Rio Tinto.

Australia is the world’s largest producer of bauxite—the primary component of aluminium. Aluminium is a key part of our everyday life and helps us travel far and wide. It is used in bikes, cars, trains and planes because it’s strong, lightweight and corrosion resistant. These properties also make aluminium the perfect solution for countless food and beverage applications—from drink cans to aluminium foil—and most importantly, it can be recycled over and over.

Rio Tinto is a global leader in aluminium, and located in Far North Queensland on Cape York in Australia, is their Amrun mine. The Amrun mine is the third continuous mining operation alongside East Weipa and Andoom in the Rio Tinto Weipa Operations portfolio, which has been producing bauxite since 1963.

Rio Tinto’s Weipa Operations exports more than 30 million tonnes of bauxite annually and Amrun, their newest bauxite mine, features the latest integrated control and automation technology from Rockwell Automation.

Smart automation and control

Constructing Amrun took three years, with automation and control requirements needing to be carefully considered with the mine being in such a remote and isolated location. The project went to market for a Main Automation Contractor (MAC) to provide engineering design services, equipment supply, implementation services, site services through offsite switch room testing, pre-commissioning and commissioning support, as well as training services. A key aspect of selecting the MAC was partnering with an organisation that could demonstrate capability in delivering an end-to-end automation solution for a major capital project. Of importance was the project delivery personnel who would see the project through from design office, Factory Acceptance Testing (FAT), pre-commissioning and commissioning.

The Rockwell Automation suite of products provided a complete solution from the ground up—from its communications stack, security, product integration, diagnostics and engineering tools as a complete solution.

The processing plant, materials handling systems, water and tailings, mine infrastructure, wharf and rail mounted machines are all controlled by Allen‑Bradley® ControlLogix® controllers, together with Allen‑Bradley CompactLogixô controllers for smaller outdoor MCCs and package controllers. Given the scale of the Amrun site, there are approximately 50 PLC controllers in operation across the site.

The Connected Mine

With a large, distributed architecture, Amrun needed a modern Process Control System (PCS) that could provide seamless integration between critical mine processes.

After looking at various technologies, a Rockwell Automation PlantPAx® solution was implemented, delivering cost savings and schedule benefits. Using a predefined and standardised library ensured rich functionality and robust performance. The usability of the PlantPAx toolset allows for quick modify configuration and its ability to be easily integrated across multiple systems has simplified control system troubleshooting.

By using a common automation platform, the PlantPAx system provided seamless integration between critical process areas of the processing plant. Amrun’s control and automation system uses Converged Plant wide Ethernet (CPwE) communications with the complete FactoryTalk® suite of products. The entire suite of application servers are virtualised on high availability data centres.

Main Image

The Rockwell Automation PlantPAx system connects critical process areas of the processing plant.

Amrun is located in an isolated site approximately 800 kilometres from Cairns, Australia. As such, the data centre is integrated into Rio Tinto’s IT infrastructure, enabling centralised management and remote access. A set of portable mobility tablets was implemented so operators could access data from the plant. These devices were enabled by ThinManager®, providing users access to real time information.

“With integrated software that can collect and manage the information from various sensors, devices and systems from across the site, operators can now collect, coordinate and share data internally. This helps to ensure better data-driven decision-making and greater consistency in results,” said Bernard Ooi, project manager, Rockwell Automation.  

Main Image

Bauxite being loaded onto a vessel at the Chith Export Facility at Amrun. Photo courtesy of Rio Tinto.

Emphasis on safety

Safety was a key priority for the mine and processing plant and as such, Amrun uses the latest technology to run operations safely and efficiently. Functional safety was implemented in GuardLogix controllers and integrated with the PLCs to provide seamless visibility of safety and control.

Early commissioning

With such a large-scale project, it was important that commissioning was a smooth process. To help achieve this, FAT was undertaken at the Rockwell Automation facility in Melbourne. The majority of the plant was staged and tested in a complete integration test to simulate the control of the plant from the dump truck through to the ship loader. The full integration test was conducted with the required controllers and application servers hosted on the VMWare-enabled data centres.

The Amrun project was delivered under budget and ahead of schedule as a result of an integrated approach to design, construction and commissioning.

“Amrun is a great example of innovation through collaboration which is vital for advancing the future of mining,” said Glenn Otway, manager, Power and Automation, Rio Tinto.

 

About Rockwell Automation

Rockwell Automation Australia and Rockwell Automation New Zealand are subsidiaries of Rockwell Automation, Inc.—a leading global provider of industrial automation and information solutions that helps manufacturers achieve a competitive advantage in their businesses. The company brings together leading global brands in industrial automation which include Allen‑Bradley® controls and services and Rockwell Software® factory management software. Its broad product mix includes control logic systems, sensors, human-machine interfaces, drive controllers, power devices, and software.

Rockwell Automation Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 23,000 problem solvers dedicated to our customers in more than 100 countries. To learn more about how we are bringing The Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com

Allen‑Bradley, CompactLogix, FactoryTalk, GuardLogix, PlantPAx, Rockwell Automation, Rockwell Software, Stratix and ThinManager are trademarks of Rockwell Automation, Inc.

 

Media contact:

Christine Filippis
Teraze Communications
61 3 8391 0701
christine@teraze.com.au

Published November 18, 2020

Topics: Mining, Metals & Cement PlantPAx DCS
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right
Company
About Us Accessibility Careers Diversity, Ethics and Integrity Engage Online Community Investor Relations Modern Slavery Statement Newsroom Sustainability Trust Center
 
Trending Topics
Cybersecurity Digital Transformation Smart Manufacturing The Connected Enterprise®
 
Our Brands
Allen-Bradley FactoryTalk LifecycleIQ Services
Events & Training
Events Training Webinars
 
PartnerNetwork
Find a Partner What is the PartnerNetwork?
Contact Us
TechConnect Support Customer Care General Inquiries How to Buy Report Ethical Concerns Customer Experience Survey
Insights
Results Achieved Blogs Case Studies Automation Today Podcasts
BlogRockwell Automation's Blog
Legal Notices
Privacy & Cookies Policy
Email Preferences
Cookie Settings
Accessibility Settings
© 2025 Rockwell Automation
Home