Loading
Blog | Process Solutions
Recent ActivityRecent Activity
2 minute read

Modernize Your Plant With High Speed Ethernet

Modernize your plant with high-speed Ethernet to the field technology with Ethernet-APL.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Female engineer monitoring field device technology digitally.

The Next Standard for Field Applications in Process Industries

Ethernet-APL™ (Ethernet-Advanced Physical Layer) enables the future of process automation through these core features:

  • Ease of adoption
  • Seamless integration
  • Simplified installation
  • Greater distances
  • Process industry rated
  • Valuable data

As digitalization becomes more common in industrial automation and companies seek to extract its value, access to data is more crucial than ever.  

However, process industries have special requirements that make it more difficult to modernize towards digital solutions. An example of these requirements include seamless and fast communication from the field to the information level in explosive and hazardous areas in harsh conditions. In this sensitive industrial sector, any deployment of new technology must be thoroughly tested along with providing added business benefits. Furthermore, new technology cannot require extensive training for installation and maintenance making meeting the needs of the process automation industry a difficult task. This highlights why it has been such a challenge to digitize the field level in the process industry—until now.

Ethernet-APL is hazard rated and purpose built to be the next standard for field level applications. It has been developed based on requirements from end user organizations like NAMUR. Along with key features like 10 Mbit/sec communication bandwidth and two-wire cabling capable of powering field devices, one of the major advantages of Ethernet-APL is how easy it is to use.  Ethernet-APL extends EtherNet/IP to all areas of process operations. This enables PlantPAx® DCS, digitalization, and expansion of the edge of the Connected Enterprise.

Why should you be interested in Ethernet-APL? Simply said: it is the future of process automation.

Ready for a deeper dive? Watch on demand how to unlock the potential of smart sensors and instruments for production facilities enabled by Ethernet-APL technology.

Tune in live to ACHEMA Pulse, a virtual global forum on June 15 and 16 of 2021, that aim to bring people, ideas, and technologies together to explore new opportunities for collaboration. Ethernet-APL will be represented at the show at an independent virtual booth that will hold a variety of business and technical live talks on the Ethernet-APL technology.

Published May 28, 2021

Topics: Process Solutions Distributed Control Systems (PlantPax)

Frank Schirra
Frank Schirra
Global Portfolio Manager, System & Solutions, Rockwell Automation
Frank has over twenty-four years of extensive work experience in process automation. In his current role he is responsible for the Single-use Bioreactor solution and is helping customers to be more efficient and accelerate time to market.
Connect:
EmailEmail
Gregory Wilcox
Gregory Wilcox
Principal Application Engineer, Innovation & Technology, Rockwell Automation
Gregory Wilcox is a thought leader with emerging communication technologies, IIoT, IT/OT convergence and cybersecurity.
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
So, you have ThingWorx but where do you start?
So, you have ThingWorx but where do you start?
Blog
So, you have ThingWorx but where do you start?
The ThingWorx application enablement platform from PTC contains the framework and features required for building any type of IoT or IIoT application.
Plant Efficiency with the Right Control Hardware
Plant Efficiency with the Right Control Hardware
Blog
Plant Efficiency with the Right Control Hardware
Universal I/O enables flexibility and allows for late modifications supporting the lifecycle of the system.
Automation Fair OEM Forum Recap
Automation Fair OEM Forum Recap
Blog
Automation Fair OEM Forum Recap
Couldn't make it to Automation Fair? Discover how our OEM Forum panelists are navigating uncertainties.
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right